Download the Application

  • Click the Compile and Download button (Ctrl + F7) or the Download button.
    The application is compiled and downloaded or just downloaded to the controller.
    • If you enabled the "Download Project Source in the controller" option in the Controller Properties dialog box (see Configure the Controller) then the source code is also copied to the controller.
    • If you disabled the "Download Project Source in the controller" option and the controller has project source loaded you will be prompted with a message. The message presented will vary, based on whether your current project and the project on the controller have the same name or not.
      Project NamesMessageActions
      Same nameOK: Source on controller is deleted.
      Save: Source on controller is overwritten and is also saved to "My Documents". If that source file already exists in My Documents you will be prompted to rename the source file, overwrite that file or not. If you do not rename or overwrite the file then the download to the controller will be canceled.
      Cancel: Download is stopped.
      Different nameOK: Source on the controller will be replaced.
      Save: Source on the controller will be saved to "My Documents" as above.
      Cancel: Download is stopped.
    • You will be prompted with an alert to connect to a controller if you try to Compile and Download without being connected.
    • You will be prompted with an alert if there is not sufficient space on the controller for the application. Clearing the User Data is one method to create more space on a AKD PDMM or PCMM.

  • In addition to downloading the application to the controller's flash memory, you can download the project's source code, allowing you to store the project. See File Menu for information on retrieving saved projects.